我是一名学生,目前在研究AFE4400的评估板,根据用户指南上的说法,AFE4490的LED_DRV_SUP和TX_CTRL_SUP应该是5V,而AFE4400的LED_DRV_SUP和TX_CTRL_SUP应该是3.3V,但是根据用户指南给出的电路原理图,并没有说明AFE4400的供电方式和AFE4490有什么不同。请问能帮助说明下用户指南的电源支持电路经过了什么改动才能适应AFE4400么?另外由于我不太懂TI的电源芯片,请问用其他方式产生3.3V和3V电压的话对设计有影响么?谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我是一名学生,目前在研究AFE4400的评估板,根据用户指南上的说法,AFE4490的LED_DRV_SUP和TX_CTRL_SUP应该是5V,而AFE4400的LED_DRV_SUP和TX_CTRL_SUP应该是3.3V,但是根据用户指南给出的电路原理图,并没有说明AFE4400的供电方式和AFE4490有什么不同。请问能帮助说明下用户指南的电源支持电路经过了什么改动才能适应AFE4400么?另外由于我不太懂TI的电源芯片,请问用其他方式产生3.3V和3V电压的话对设计有影响么?谢谢。
EVM中的5V和3.3V的LED_DRV_SUP和TX_CTRL_SUP都是通过TPS61093输出的8.97V经过LDO LP3878-ADJ产生的。 LP3878-ADJ的输出范围为1V~5V。 你可以参考下LP3878-ADJ的datasheet中介绍的如何设定输出电压:
http://www.ti.com/lit/ds/symlink/lp3878-adj.pdf
你好,我最近在研究心率监测,在AFE4490评估板的电路图(TIDA-00010)太不清晰了,能否提供给我一份清晰版的原理图。邮箱:113344dd@163.com
另外 因为看不清所以不知道电路图TIDA-00010和TIDA-00011有什么区别,所以如果有差异,能否都发一下给我。谢谢
AFE4490的LED_DRV_SUP和TX_CTRL_SUP必须要接到5V吗? 连接3.3V是否可以?会出什么问题呢?
电路图在附件的EVM user guide里面有,太大了传不上来。
你去官网搜索“AFE4400 and AFE4490 Development Guide”
文件编号“SLAU480A”