This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1248 校准

我用一个定值为120欧姆的电阻来来代替PT100,但是测量出来电阻值为123.49,我想通过校准把误差缩小一点,请问该怎么做

  • 您好,

    出厂前是有一定的Gain校准的,芯片也提供系统级校准。Offset分系统校准和芯片自身校准。系统级校准System Calibration,手册里有专门章节写,需要提供满量程信号和0输入时候的信号,写入校准命令。自身校准只有offset的校准,只需要写入校准命令即可。

    以上是关于芯片自带的校准,以下主要说明下其他的校准方法。

    我想知道您的120欧电阻本身精度是多高的? 用了多高的精度万用表进行测量出的120欧? 

    另外就是您的计算公式里使用的Vref值是理论2.048V还是在Vrefout的值测出带入计算。如果使用测出的值应该能更加提高精度。另外就是根据我的经验,不校准情况下应该也能到万分之几精度,也不至于差到3%左右,所以我想知道你的120欧电阻真是120欧吗?