This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于ADS62P49输入和DAC5682Z输出的问题

Other Parts Discussed in Thread: ADS62P49, CDCE72010, DAC5682Z, LMK04906

各位好,我最近想用ADS62P49和DAC5682Z两款芯片做相关设计,经过了解数据手册和评估板手册,我对ADS62P49的数据输出及DAC5682Z的数据输入有了确定的连接。但对AD的模拟输入和DA的模拟输出方面的设计还不太确定,问题是我在前端想用射频芯片MAX2829,该芯片对AD有两对差分输出、对DA有两对差分输入,我能直接将MAX2829的差分输入、输出按照ADS62P49、DAC5682Z EVM中的变压器耦合输入、变压器耦合输出的方式做电路连接吗?能否这样连接主要是看什么指标呢?还有,如果我想由一块时钟芯片同时为这两个AD、DA提供时钟的话,用CDCE72010可以不?多谢解答?

  • 你好,

    第一个问题,你需要注意MAX2829的基带输入范围和接受基带输出范围是否与ADC和DAC芯片的输入输出范围是否兼容,必须接收信号大小在ADC量程内和DAC的输出不能太大(把变压器计算在内)。同时也需要考虑变压器的带宽和平坦程度,这个取决于你的系统。欢迎牛人补充。

    第二个问题,您可以下载TI的时钟设计软件Clock Design Tool。里面可以仿真计算出各种时钟需要的参数例如相噪或者抖动,然后可以查看是否满足。

  • 您好,我在做设计时,对于ADS62P49的时钟输入,我计划用LVDS形式,通过手册发现要求CLKP/CLKM电压范围是-0.3V-AVDD+0.3V,LVDS VPP为700mV。这是不是表示常见的例如350mV的LVDS标准不能应用呢?若要使用ADS62P49的LVDS时钟输入,应该怎样设计?还需要注意什么?有什么参考文件吗?

    对于DAC5682Z,它的时钟输入CLKIN/CLKINC可以采用LVDS输入码?应该怎样设计?因为我看CLKIN/CLKINC的电平要求是differential voltage 0.5--1V,input common mode voltage的典型值是0.9V,也不是太符合常见LVDS设计的要求?我应该怎么办呢???

  • 时钟推荐使用LMK04906, 提供更灵活的频率和更低的功耗,相关的连接匹配电路参考手册如下;

    http://www.ti.com/product/lmk04906