Other Parts Discussed in Thread: SN74AVC8T245
Hi,
I am using sn74avc8t245 as voltage shifter from 0~3.3 V to 0~2.4 V, I have three questions regarding this part:
1. How should I connect the pins (i.e VCCA, Two VCCB, DIR, OE)
2. What does continuous output current mean (under absolute maximum ratings on page 3)? What is the difference between continuous output current and IOH/IOL?
3. Is this part able to drive a 50 Ohm resistor? If not, do you know any part can drive 50 Ohms with a voltage level of 0~2.4?
Many thanks in advance!
Miao