各位专家好!这边想选择一款能够实现多个通道数据采集的ADC,由于对通道间的幅度和相位一致性要求较高,最好可以严格控制各通道之间的同步,要求单个通道的吞吐量为1MSPS以上,SNR最好在90dB以上,分辨率至少16位,且16位最佳,接口最好为串行接口。谁能帮忙推荐几款这样的ADC吗?或者有其他好的方案可以推荐吗?谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
现在的多通道同步采集系统是采用单个多通道ADC对每个通道进行同步采集还是采用多个同型号的ADC对每个通道进行采集,这两个方案的优缺点您知道吗?需要16路同步采集,单路采样率在1MSPS以上,好像对于那种多通道的ADC这个采样率有点高呢,谢谢您的回复
如果你做多通道同步采样,那么用多通道的ADC比用多个单通道的ADC在集成度,成本,通道一致性,和系统设计上会有优势.一般的话500K应该差不多了,采用ADS8568的非常多.你可以研究下
嗯,好的,这个ADS8568的输入类型好像是单端的,这边可能想用差分信号作为输入,请问有类似的多通道差分输入的ADC吗?
Please check ADS8555/6 and ADS8361/3
谢谢您的回复,我查看啦您推荐的ADC,ADS8555/6每个通道都有一个采样保持电路,可实现最多6个通道的同步采样,但是输入为单端双极性输入,如果要使用的话就需要在我前端加一级差分转单端啦,但是这边不希望改动前端电路,所以要求最好为差分输入的ADC,ADS8363可以作为4通道差分输入ADC,但是内部使用了MUX,只能实现2个通道的同步采样是吧?如果我要使用ADS8363实现4路差分信号同步采集,是否需要使用2个ADS8363呢?