Other Parts Discussed in Thread: ADS1258
小弟现在,正在调试ADS1258这款芯片,前期所有的调试已经结束,采集数据包括读寄存器都正确,不过在跟系统联调时,由于系统工作不正常,导致我们的板子上的一个-15V的滤波电容直接烧爆了,应该是瞬间电压过大导致的,后来我们跟系统解调,自己给板子单独供电,但是这时候ADS1258芯片就出问题啦,在外面信号线都不接的情况下,采集到的数据是-2.417V,不过这时读内部的寄存器VCC,REf都是正确的,而且可以通过SPI通信向芯片内部写命令,就只是采集到的数据不正确,到现在都搞不清楚到底是怎么回事,小弟弱弱的问一下,我现在的观点是,是不是ADS1258芯片的多路复用器被烧坏了,因为在系统联调时,这些采集信号线是一直跟系统接着的,是不是系统瞬间产生过大的电压,把多路复用器烧坏了,而芯片的其他部分确是正常的,导致现在采数据16个通道的数据都是-2.417V,也就是说ADS1258的不是整体烧坏了,而是只是烧坏一部分(也就是多路复用器),请问一下你们遇没遇见过这种情况,我可不可以这么理解?
小弟急求,在线等,在这里先谢谢啦!