Other Parts Discussed in Thread: ADC14L020, ADS5240
各位老师好:我想选择一个单通道或者4通道的ADC。要求采样率为20M以上,价格不要太贵的,请各位老师给推荐下。谢谢了!
还有一个问题是ADC芯片的interface有Parallel LVDS与Serial SPI Interface与Parallel CMOS之分,各代表什么意思,哪一种性能好呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你对ADC的精度要求是多少位?
ADC数字接口不会影响ADC的转换性能,主要看你外部主控有哪种接口来对接ADC。对于高速,像>20M的话,Serial SPI可定不能用了,一般用LVDS,或parallel coms的接口。
4ch的可以选ADS5240,单通道的选ADC14L020,性价比很高。
如果是LVDS的话,估计ARM接不了。ADC14L020是并行CMOS/TTL,不知道你用的ARM I/O翻转速度有多快?
一般我们都是用FPGA来接高速ADC的。
老师您可以具体讲一下,ADC芯片的interface有Parallel LVDS与Serial SPI Interface与Parallel CMOS代表什么意思吗?或者有参考资料可以推荐看看!谢谢了!
这些都是标准的东西, LVDS是一种低压高速差分电平标准,CMOS类似于TTL的单端电平标准, SPI类似于I2C通信接口,你可以分别百度下,很多相关的资料,也很容易理解。