请教专家:
我现在手上有一个线圈,但没有阻抗分析仪,怎么样才能测得到此线圈Rp_max、Rp_min和谐振频率?视频中测量这三个参数时,也需要和LDC模块连接起来吗?谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请教专家:
我现在手上有一个线圈,但没有阻抗分析仪,怎么样才能测得到此线圈Rp_max、Rp_min和谐振频率?视频中测量这三个参数时,也需要和LDC模块连接起来吗?谢谢!
Hi Sally,
Impedance analyzer is not required, it just provides a more scientific way of tuning Rp min/max values for optimal performance.
You should connect LC circuit with LDC use an empirical way of Rp tuning:
1) Set Rpmin to 3F, RpMAX to 0.
2) Expose the coil to the maximum metal coverage for your application (closest target position, thickest part etc)
3) Start reducing RpMIN setting 1 code at a time, and take Rp Measurements (they will go up with each change).
4) When Rp gets in the range of 20,000 - 30,000 codes, that is your optimal RpMIN setting.
5) Move your target to a position where it's exposed the least (farthest position, thinnest part) etc.
6) Start increasing RpMAX setting 1 code at a time, and take Rp Measurements (they will go down with each change).
7) When Rp gets in the range of 2,000 - 3,000 codes, OR the difference between RpMIN and RpMAX values reaches x25 - x26, that is your optimal RpMAX setting. It may get too noisy, then back off 1-2 RpMAX codes.
P.S To speed up tuning, you may change the codes by more than 1 code at a time, for example - binary search etc.