各位大虾同仁们,小弟设计了一个ADC14L040的电路,按照数据手册,其参考电压应该是1V(我用的是内部参考,电路解法基本参照手册),可是在实测中为1.5V的直流参考,请问这是为什么?还有,ADC14L040的内部有保护电路吗,当我的输入峰峰值超过4V时,采集出来的数据是上下不对称削幅!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Qiang,
你看一下数据手册第18页,VRM是参考旁路的管脚,并不代表参考电压,他就是1.5V输出。
The nominal voltages for the reference bypass pins are as follows:
VRM= 1.5 V
VRP= VRM+ VREF/ 2
VRN= VRM− VREF/ 2
Hi Qiang,
每一路的输入峰值不超过2.6V可以理解为最大值是2.6V,应该是由于电源供电电压的限制,并不代表差分最大是5.2Vpp。
因为共模的关系,所以输入信号可以最大值可以2.6V,最小值为0.6V,这样峰峰值就是2V。
最大值2.6V,最小值0.6V只是举个单端的例子。对于差分信号,只要共模电压设置合适,最大值也能到2.6V。
对于1.0V的参考,full scale的输入范围就是2Vpp。
2:共模电压VCM范围是0.5-2.0v,这个电压设计者怎么提供?没有VCM管脚呀。
A: 确实没有Vcm管脚,但是Vcm是输入信号的共模电压,比如0~2V的信号,加上Vcm=1.5V 参考的话,就是1.5V~3V的信号。
3. 准备用单端输入模式,输入信号是0-2v,是不是把参考电压设置为内部1v参考电压,VIN-端和VCM都接到1v即可?VCM怎么提供、?没有输入管脚。
A: 单端输入的话,按照你说的,如果打算输入共模电压Vcm=1V的话,那么就将Vin-接在1V即可。1V可以是前端比如全差分运放的Vom,也可以是LDO的输出电压等等。