This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于ADS41b25输入输出问题,请教各位大神



cmos输出模式下,INP接信号端,INM接地,输入电压0-1.5V直流电压,电压由基准通过运放给出。

当我输入0.8V~1.5V时,输出值由830~fff变化,可以确定输出值时随着输入电压的增大而增大的,但是越靠近两端变化越不明显。
当我输入0~0.8V时,输出值在800~830之间变化,虽然也是随着电压增大而增大,但是幅度太不明显。
是因为0~0.8V不在测量范围吗?可是溢出标志位也没有输出“1”;
当输入电压大于1.5V时,溢出标志位输出“1”
这种情况是由什么原因引起的,是硬件电路的原因还是寄存器配置不对?