Part Number: TLV5638M
Other Parts Discussed in Thread: TLV5638
TLV5638MJGB这个器件 一共装机36片
有1片,输出有问题。具体描述如下:
TLV5638,正常VREF (OUTL) 正常输出1.024V,范围1.003V到1.045V,现在有问题这片输出为0.980V
还有一片输出1.008V,虽然属于正常范围,和1.024V相差较大
其它34片输出基本在1.020V到1.025V之间
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,TLV5638上电后,有两片Vref输出误差较大是吗?还是说工作一段时间后发现输出有误差的?
做交叉实验了吗?将有问题的芯片换到正常工作的板子上,验证下是板子的问题还是芯片的问题?
您是在哪儿购买的?