Other Parts Discussed in Thread: ADS7263, ADS8363, DAC8564, DAC8168
1.DAC要求 16bit 4/8通道,每个通道的采样率在500khz到1mhz之间
2.ADC要求,14/16bit,4/8通道,每个通道的采样率要求为1MSPS
大神求回复啊
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
ADC你可以看看
ADS7263 1M采样率,14bit,4通道
ADS8363,1M采样,16bit,4通道
Seasat ,很感谢你的答复,对我帮助很大,C8868芯片好像不存在,是不是写错了
Seasat,你好,还有个问题,ADS7263,ADS8363每个通道都是1M采样率??
我开始以为1M采样率,又是串行端口,那采样率就成了1M/4(通道数)/16(串行输出),这样考虑应该是不对,那应该怎么考虑?
Carter,很感谢你的帮助,我想问下,TI的芯片说的采样率是指的单通道还是多个通道同时工作时的采样率,这要怎么看?
不好意思,笔误。
DAC8168 14-Bit, Octal Channel, Ultra-Low Glitch, Voltage Output DAC with 2.5V, 2ppm/°C Internal Reference
多通道的ADC有同步采样和非同步采样两种。同步采样就是内部有多个ADC,每个ADC的采样都是独立的,采样率也一样。非同步采样是分时复用的,每个通道的采样率就是总采样率处以通道数