Other Parts Discussed in Thread: DAC908
Hi
DAC908输出不对 我的板子按照DAC908 datasheet上的典型接法,使用内部基准1.24V, IOUT端和/IOUT端都对地接了24.9R的电阻,发现当给DAC908的8位数据接口发送128时/IOUT输出500mv,IOUT输出为0,当发送127时IOUT输出为500mv,/IOUT输出为0,根据datasheet上的计算公式,发送128时,IOUT和/IOUT都输出10mA的电流,在电阻上的压降都为250mv左右,但是实际测试结果显然和datasheet上说的不对啊,好像实际测试,发送128时,/IOUT端输出20mA电流,IOUT输出电流为0
看起来像是补码而不是datasheet上描述的二进制码?