Other Parts Discussed in Thread: ADS5263, PGA870
准备使用ADS5263设计一个AD采集卡,遇到了下面两个问题,还请大家多多指导。
1. 16位模式,4Vp-p,但是Voltage applied to analog input pins – INP_A, INM_A, INP_B, INM_B –0.3V to minimum (3.6, AVDD + 0.3 V) V,3.6-(-0.3)=3.9,如果是4Vp-p输入,必然超出芯片输入绝对最大值?
2. 前端差分驱动用哪个好,因为ADS5263差分输入共模电压要求1.5V,可否由PGA用+4V和-1V电源来驱动使得PGA870输出共模电压为1.5V?
请指教,谢谢!
另:如何保证前面差分驱动器输出的信号不超过ADS5263的量程?