Other Parts Discussed in Thread: AFE5808
利用TSW1400和AFE5808AEVM进行测试,测试过程中我想用板载CMOS时钟,所以J9跳线帽连了OSC,在AFE5808AEVM的软件中的ADC模块选择了Single Ended和ramp,在HSDC Pro中选择的AFE5808_14X利用HSDC pro进行Capture,报错如下所示。我想问一下这个是什么原因造成的呢?如何判断是哪里出了问题?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
利用TSW1400和AFE5808AEVM进行测试,测试过程中我想用板载CMOS时钟,所以J9跳线帽连了OSC,在AFE5808AEVM的软件中的ADC模块选择了Single Ended和ramp,在HSDC Pro中选择的AFE5808_14X利用HSDC pro进行Capture,报错如下所示。我想问一下这个是什么原因造成的呢?如何判断是哪里出了问题?
Ramp Test的话,应该不需要修改电路板。
选择 AFE5808_14X的时候是选择的带 MSB的吗?
另外,下面帖子操作步骤希望对您有参考帮助:
只有“AFE5808_14x”这个,那就是选这个。
您是否可以测量下JP9的3脚是否有时钟信号?
您是否有办法测量下P10-58 和 P10-66 是否有时钟信号?
最后确认下实测下TSW1400EVM的供电电压5V电压是多大?下面帖子说这个5V电源需要提供至少3A的电流,否则的话会出现上述错误: