Other Parts Discussed in Thread: DAC3482, DAC3283
在DAC3482中,采用片内混频器实现上变频功能需要保证两路输入信号的正交性么?现在想用DAC3482将两路不相关的基带信号转换成中频信号输出,能否实现?请详细说明一下信号处理过程
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Wu
3482就是把输入的信号与正弦和余弦向乘,然后积画和差,然后滤波。
不相关的基带信号转换成中频,你的意思是用混频器输出吧
是这样,现在的应用是想利用3482实现数字上变频,我看手册上混频结果将IQ两路输入信号混在了一起,这样在IQ两路输入信号没有任何关系的情况下,混频器的输出不就影响输出信号的正确性了么
IOUT(t) = (IIN(t)cos(2πfNCOt + δ) – QIN(t)sin(2πfNCOt + δ)) × 2(mixer_gain – 1)
QOUT(t) = (IIN(t)sin(2πfNCOt + δ) + QIN(t)cos(2πfNCOt + δ)) × 2(mixer_gain – 1)
如果要实现正交上变频,是必须要用到I路和Q路信号的,。如果I路和Q路本身没有任何关系,就不能使用正交上变频,就要考虑普通的混频器了。3482里面的是叫调制器,是需要IQ。不需要IQ的是叫混频器
如果你要两路dac出信号信号则不能使用调制功能。如果需要调制请参考DAC3283手册PG34, Table6的前两个模式
Coarse Mixer Sequences
Mode mixer_func(1:0) Mixing Sequence
Normal (Low Pass, No Mixing) 00 AOUT = { +A, +A , +A, +A }
BOUT = { +B, +B , +B, +B }
fS/2 01 AOUT = { +A, –A , +A, –A }
BOUT = { +B, -B , +B, -B }