芯片的数字信号输出有二进制补码和二进制偏移码两种形式,请问如果输入端(Vin+)—(Vin—)分别等于0V、1V、2V时对应的数字输出是什么呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,首先数字信号输出是二进制补码形式还是偏移码形式可以通过加在DFS pin上的电压进行配置,也可以通过寄存器进行配置。
DFS的电压配置参考Table 7:
寄存器配置是寄存器3Dh的bit7:6
您指的输出code具体为多少是吗?
ADS4149的典型差分输入为2Vpp,14bit的话1 LSB = 0.12207mV。1V输入的话输出code为8192.