请问 4-20mA 的电流信号怎么转为 0-3.3V 的的电压信号给进ADC?有什么芯片或模块的解决方案吗?谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
这种是最简单的方法,串一个 150欧 的电阻输出的电压范围是0.6V - 3V,网上也查到说这种方法不太精准,请问有没更好的方法,最好就具体的电路,谢谢。
TI只有一款4~20mA的接收器,RCV420,输入4~20mA,输出0~5V。
可以参考10uA-10mA 转100mV–4.9V的参考设计,把增益调整一个就可以。采样电阻的精度很关键。
http://www.ti.com/tool/tipd104?keyMatch=10%C2%B5A-10mA&tisearch=Search-EN