Other Parts Discussed in Thread: OPA132, ADS7862
按照datasheet中的典型应用电路,用一块OPA132运放,完成±10V的模拟输入,用一块有源晶振输出4MHz和200khz分别作为CLK和convst,IO口模拟RD和CS,进行数据采集,采集结果只能收到-10v~0v输入所对应的的800~fff,而0~+10v输入,采集到的一直都是fff
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
能不能把ADS7862输入口的电压用示波器量一下?看看输入的波形是什么
最靠近ad输入管脚的电压是直流电平,即IN+与IN-之间是-2.5V~+2.5V的电压。我的邮箱是heshanshan365@foxmail.com咱们能用邮箱交流吗?
所以在直流+6V输入的时候,CH B0+ 为+4V, CHB0- 为+2.5V, 而ADS7862转换结果为FFF?
读取时序以及通道选择方面有咩有问题? FFF意味着0输入,倒像是其他没接输入信号的通道的转换结果!
dear Martin:
关于之前的问题,我把+VD接3.3v改成5v,问题已解决。0~+10v的输入也能读到正确的值。现在又出现一个新问题!
我把A0接地,让芯片只采集CHA0,CHB0两个通道的数据,电路板上CHA1,CHB1都是悬空。读数据时数据会在两个通道互窜。CHA0给一定模拟输入,CHB0给模拟0v,有时读取两个通道数据会一样,有时接1通道,在另一通道读到的数据。您看怎么解决这个问题。