This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于ADS1110的使用问题,希望有TI的FAE技术支持,谢谢!

Other Parts Discussed in Thread: ADS1110

项目在调试阶段,发现将VIN+/VIN-/GND三端短接一起,软件设置15SPS;PGA=1;IIC还能读到AD值为0X0033H;若将PGA=8;IIC读到的值会更大,请问这个什么问题?

  • 你的供电质量如何?电路板布线如何?测试周围有很大的噪声源吗?

    测试多片ADS1110都是这个情况吗?

  • Martin,你好!供电是采用可调稳压电源提供7V以上,经过板子的78M05稳压,周围没有大噪声源,测试过两片,情况一样,昨天上电还是我讲述的0X0033H,今天上电,AD值就降到显示为0X0003H,要说明一下,程序问题可能性不大,因为我将V-接地,V+给2.047V以下的电压,显示值(我将AD用4数码管显示出来)会跟随输入的电压变化,实际显示值与理论值相近,实际显示值与理论值之差,几乎就是VIN+/VIN-/GND三端短接一起,仍然有的AD值;


  • Martin,你好,供电时采用可调稳压电源给7V或以上,供到板子上的78M05,布线方面ADS1110与电源地很近,周围没有大的噪声源,测试2片ADS1110情况一样;但昨天上电是我讲述的0X0033H,今天上电显示的却是0X0003H,说明一下,程序问题可能性不大,我将AD值用4位数码管显示,200ms刷新一次显示;我试过将V-、GND短接一起,V+给2.047V以下电压,显示的AD值会跟随电压变化;而且实际显示值接近理论值;

  • 0x0003H的话就是正常的了,有偏置电压嘛

  • 建议调试的时候将数据都读出来看看,200mS刷新一次的话是不是已经滤掉很多次转换的结果了呢?

  •  你好,Martin,我之前回复你说,显示由原来的0X0033H变成了显示为0X0003H,我找到原因了,并不是电路正常了,只是我将DATA RATE的速度,由15SPS,改成了240SPS,根据资料,输出的数据的位数也会由16BIT降低为12BIT,相当于0X0033H右移了4BIT而已,即现在显示到的0x0003H,PCB板已经做了,不是之前的手工感光板了,线路问题可能性不大;这0x0033H是哪里来的呢?是内部运放的失调电压导致的吗?那就是说,输入是0V,输出不是0V,那我后面输入其他电压,例如100MV,读到的AD值,要不要减去这个0X0033H呢?

  • 16位输出的时候,0X0033H 换算后等于 3.18mV。 在ADS1110的失调电压范围,确实是由PGA和ADC的失调电压引起的。

    这个失调电压会导致 输入是0V,输出不是0V。你可以在软件上做校准:在后面输入其他电压,读到的AD值,再减去这个0X0033H。

  • 请问下,我用ADS1110测量,V-接GND,V+接输入电压,这样测得的正电压没问题,但测得的负电压小于-200mV,就会偏差很大了,难道这样接测差分电路是不行的吗?

  • 你的意识是负电压,大于-200MV是准确的,但小于-200MV偏差就大,还是说负压就有很大偏差,一般测负压,V-端就不能与IC共GND,不知道你现在是不是这个原因~

  • 你好,我最新使用了ADS1110 ,ED0,ED1,ED2,    其中ED0 ,和ED2能按照手册地址正常读写,但是ED1 ,不能按照手册地址读写,但是ED1,能按照ED0的地址读写,芯片封装上可以很清晰的看到,ED1,不知道咋回事,求帮助啊