Other Parts Discussed in Thread: ADS5263EVM, ADS5263
各位专家,你们好,我测试用的是TI公司的ADS5263EVM开发板,目前有以下问题,急需解决:
(1)只给板子上电,不提供采样时钟输入,有帧时钟,位时钟,和数据输出。其中帧时钟为几百HZ占空比不为50的方波,位时钟为几KHZ占空比不为50的方波
(2)对板子上电,提供采样时钟,不提供信号输入,帧时钟,位时钟输出正确,有数据输出
(3)EVM开发板提供了板子的原理图,原理图与ADS5263数据手册,有三个管脚对不上,比如说datasheet中有SDOUT,而开发板原理图中对应管脚为NC,还有两个管脚datasheet中为NC,但原理图中有东西
(4)ADS5263一定需要寄存器配置才能使用吗?默认模式下,是不是帧时钟输出为1X,位时钟为8X,数据输出为16为串行码,如果这样的话,可以不需要配置寄存器?寄存器配置下电应该无效,再上电恢复默认状态吧?
(5)根据datasheet,默认模式下,A端口为16位模式,B端口为14位模式,无论信号从A还是B输入,输出都应该在2,4,6,8通道,但是我现在对IN3A输入,信号输出却在5通道
(6)我现在使用开发板,外飞线至FPGA板进行寄存器配置和解串,采样时钟为10M(最低),信号输入为1M占空比为50%的方波,输出5个FFFF和5个0000,但是将占空比改为60%后,输出就会发生错误,会有4F86这种数据出现,100个16位数据估计才会出现4个FFFF和6个0000的情况,其余全部是错误数据
由于这些问题的困扰,请教各位前辈不吝赐教,谢谢