Other Parts Discussed in Thread: ADS1248
用的SPI2与ADS1248相连
ADS1248WREG(ADS1248_REG_MUX0,0x01); //00100101,Bit7-6:传感器电流源检测不使用,Bit5-3:正输入为AIN0,Bit2-0:负输入为AIN1
delay_ms(20);
ADS1248WREG(ADS1248_REG_MUX1,0x30); //00110000,Bit7:启用内部晶振,Bit6-5:内部基准一直打开,Bit4-3:输入基准为片上基准,Bit2-0:普通模式
delay_ms(20);
ADS1248WREG(ADS1248_REG_VBIAS,0); //00000000,Bit7-0:偏置电压选择关闭(默认)
delay_ms(20);
ADS1248WREG(ADS1248_REG_IDAC1,0xFF);//11111111,Bit7-4:断开内部第一恒流源的连接,Bit3-0:断开内部第二恒流源的连接 0X8F打开第一内部恒流源
delay_ms(20);
ADS1248WREG(ADS1248_REG_IDAC0,0x00); //00001000,Bit7-4:只读,Bit3:DRDY/DOUT功能复用Dout线 ,Bit2-0:关闭内部恒流源
delay_ms(20);
q=ADS1248RREG(ADS1248_REG_IDAC1);
printf("4d%x",q);
ADS1248WREG(ADS1248_REG_SYS0,0x09); //00000000,Bit7:必须设置为0,Bit6-41:选择128倍增益,Bit3-0:选择2000SPS测量速度
delay_ms(20);
4d 后面回的指令都是对的