This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1298: ADS1298电路异常

Part Number: ADS1298

Hi  TIer,

    我正在调试一块自己做的PCB板子,目前遇到一些问题。我的板子的供电时AVDD=2.5V,AVSS=-2.5V,DVDD=3.3V。目前只焊接了ADS1298供电的电源部分,模拟输入部分未焊接(是否影响芯片正常工作?),数字接口RESET通过10K电阻拉高(电路图未标识),START拉高(电路图未标识),PDWN拉高,CLKSET拉高(电路图未修改),DAISY_IN通过10K电阻拉低。其他管脚SPI接口全部悬浮。

在我第一次上电后可以观察到AVDD电流1mA左右,AVSS电流1mA左右,DVDD电流小于1mA。第二次上电后发现AVDD电流缓慢变化为4mA,AVSS电流直接上升到10mA,DVDD电流1mA.

1.根据datasheet absolute rating 电流超过10mA,可能损坏芯片,请问这个芯片还能正常工作吗?

2.根据我的测量:VCAP3=3.0V,正确的数值应该是AVDD+1.9V=4.4V。是不是内部的charge pump电路工作异常?如果我设置为内部clk (clksel=1),charge pump应该可以正常工作。

3.根据datasheet absolute maximum ratings AVSS to DGND 应该在-3V~+0.2V之间,如果我使用万用表测量DGND与AVSS之间的电阻,因为测试电阻时万用表会给两端加入电压,这个电压如果超过+0.2V是否会导致芯片损坏?

这个是我的原理图,帮忙看一下是否有问题。

非常感谢!