Other Parts Discussed in Thread: TVP5160
用TVP5160做AV转YC信号,用示波器发现TVP5160的14.31818晶振不起振。
请问大概是什么原因导致的不起振。是否需要特殊的一些初始化操作才能让晶振起振?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TVP5160
用TVP5160做AV转YC信号,用示波器发现TVP5160的14.31818晶振不起振。
请问大概是什么原因导致的不起振。是否需要特殊的一些初始化操作才能让晶振起振?
hi JSW,
请检查下晶体选型和电路设计。
1)参考TVP5160的器件手册P98,晶体的指标是:标称频率14.31818MHz,频偏允许范围+/-50PPM。可以尝试换颗晶体试下?
2)电路设计参考器件手册P22,注意正确选择外部的电容和电阻参数。电容关系是CL1 = CL2 = 2CL – CSTRAY,电阻推荐是100Kohms。 谢谢。
best regards,
Steven
3.16 Clock Circuits
An internal line-locked PLL generates the system clock (SCLK). A 14.31818-MHz clock is required to drive
the PLL. This may be input to the TVP5160AM1 decoder on terminal 5 (XTAL1), or a crystal of
14.31818-MHz fundamental resonant frequency may be connected across terminals 5 and 6 (XTAL2).
Figure 3-8 shows the reference clock configurations. For the example crystal circuit shown (a
parallel-resonant crystal with 14.31818-MHz fundamental frequency), the external capacitors must have
the following relationship:
CL1 = CL2 = 2CL – CSTRAY
where CSTRAY is the terminal capacitance with respect to ground, and CL is the crystal load capacitance
specified by the crystal manufacturer.
Figure 3-8 shows the reference clock configurations.
NOTE: The resistor (R) in parallel with the crystal is recommended to support a wide range of crystal types. A 100-kΩ resistor
may be used for most crystal types.
Clock source frequency should have an accuracy of ±50 ppm (max).