Other Parts Discussed in Thread: DDC112
各位前辈们好:
我打算用ddc112采集数据,目前遇到了如下几个问题:
(1)外部积分电容。因为要采集的电流最大能大过2uA,所以打算采用0.01uf的电容。虽然datesheet写着最大电荷量1000pc限制,但是ti官方(如何在112上使用外部电容)或者第三方文档都说明到0.01uF这个外部电容也基本可以正常工作。试问有没有其他使用过这么大电容的经验,这么大真的可以用么?还有电容使用误差5%的0805的COG电容带来的误差可以接受么?还是一定要用高精度CB14电容?
(2)时钟匹配。我用的AVR单片机主控,ddc112和avr分别用各自独立的10MHz晶振,但技术文档第九页写着clk上升沿信号和conv信号要在10ns内同步,我用这种两个晶振的做法是做不到的,预计误差在几十ns,这样会带来的后果是什么?看到前面有用msp430这种与avr同档次的单片机做主控的,他是怎么做到clk上升沿和conv匹配的呢。还有关于DXMIT信号与数据输出30ns的时间限制,这些都对单片机的反应速度提出了极高的要求。是不是只有采用fpga或cpld才能解决上述问题?
渴望得到您的答复,谢谢