Other Parts Discussed in Thread: DAC8760, MAX660, LM1117, ADS8332
我使用DAC8760,不用HART模式,把DAC设置成输出1.5V直流电,设置后,发现输出在1.5V上以正弦波震荡,峰峰值为300mV,设为其他电压值也有此现象,但在0.6V以下都无此现象。下图是示波器采集到的波形,因为把示波器设为交流模式,所以显示时去除直流分量1.5V, 均值显示为0。
下图是我的原理图DAC部分,是否有问题? 我比较过此图和别人的电路图,发现一个可疑点在于,HART-IN管脚,人家的图是用一个22nF的电容连接在HART-IN管脚和地之间(前提是不用HART模式),我在设计中是悬空(因为软件上,我不设置为HART模式,而且此芯片初始值也是直流输出)。我后来试过用电容,但连接分别是1nF, 10nF和0.1uF的电容,但问题依然存在。