Other Parts Discussed in Thread: ADS4246, ADS1216
各位大侠,
目前正在使用TI的ADC,型号为ADS4246,其中有一个引脚VCM为ADC参考电压输出引脚,可以用来提供外部模拟的Bias电压。使用中发现电路板上电后,在VCM外部不接任何负载(除去耦电容)的情况下,使用万用表测试,发现其电压会逐渐下降,最开始为0.95V,然后就逐渐下降,最后大概降低至0.28V左右。但是,datasheet上表示VCM应该为0.95V左右,同时其驱动能力可达4mA。那么用万用表测试的过程中,VCM为什么会逐渐下降了?使用示波器测试也出现同样的现象。不知道哪位高手帮忙解答下,谢谢