Other Parts Discussed in Thread: OPA836

运放一算,好像最终输入AINP的值不是VIN,是2FSR_ADC-VIN,这怎么控制啊
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,Vin-Vcm=Vcm-Vout
因此Vout=2Vcm-Vin
假如Vin为0~1V的正弦波输入,Vcm=2.5V,则Vout=5-Vin
如果Vin是0~1V输入,则输出为4~5V输出,以4.5V为参考。
这个电路图的目的是为了OPA836的输出满足ADC的输入,通过Vcm将VIN的信号抬高,OPA836的输出相位和Vin相位正好相反,因为是反相输入。仿真如下,可以看到以4.5V为参考。