Part Number: ADS1299
ADS1299目前使用250 SPS , Bandwith約65 Hz
如果要量測到α β θ δ 等波段是否需加filter才能清楚看到波型
如delta (0.5–4 Hz), theta (4–8 Hz), alpha (8–12 Hz), beta (12–30 Hz)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.