DAC选型咨询:
1.单路电压输出,电压输出范围0~20V。
2.IO的电源供电最低能支持2.2V。
3.要求低功耗,静态电流要低。
4.电压输出要能够支持5mA的驱动能力(当达到5mA时脉冲宽度不超过10ms)。
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
看下DAC61402:
1 、它是双通道的,输出电压范围有:±5V、±10V、±20V、5V、 10V、20V、40V,但是请注意DAC输出电压范围一般都有headroom和footroom,也就是说输出运放输出达不到电源轨,如下截图所示:
2、IOVDD电压范围:1.7V 至 5.5V,满足要求。
3、Power-down电流±10uA,或者说20uA;
4、支持5mA的驱动能力
当达到5mA时脉冲宽度不超过10ms
这里是什么意思?
满足以上输出电压范围的且数字电压支持2.2V的 只有 DAC81402和DAC61402,它们都是双通道的,DAC81402是16bit的,DAC61402是12bit的。
如果这这两款不满足您的要求,再没有其他DAC推荐给您了。
就是说产生的脉冲宽度不超过10ms
您是说Output voltage settling time 吗?不超过10ms:
收到,谢谢!我读读这两个芯片手册
好的,有疑问您可以在这里反馈