Other Parts Discussed in Thread: DAC1280
您好。问一下DAC1280的问题,谢谢啊。
我想输出差分值为5V的电压,TDATA的占空比达到75%就行了么?TDATA的周期有限制么?datasheet中说1s density 75%,是表明按照时序把TDATA的周期设为1s,然后TDATA的占空比为75%,这样就可得到电压差分值为5V么?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: DAC1280
您好。问一下DAC1280的问题,谢谢啊。
我想输出差分值为5V的电压,TDATA的占空比达到75%就行了么?TDATA的周期有限制么?datasheet中说1s density 75%,是表明按照时序把TDATA的周期设为1s,然后TDATA的占空比为75%,这样就可得到电压差分值为5V么?
恩,昨天把datasheet好好的看了下。
按照 图一的时序编的程序
图1
也就是sync先低再高,在第四个clk的上升沿把tdata拉高,高电平持续两个clk,这样tdata的高电平数据就被采样,然后再间隔16个clk之后再拉高tdata,下一次也也是一样,这样DAC1280就连续采样到三个‘1’,再间隔16个clk之后,就把tdata拉低,同样持续两个clk,这样采样的第四个数据就是‘0’,然后重复上述步骤,一直循环。这样就可得到每次采样的数据包含3个1,一个0,满足了75%这个要求。但我昨天测了一下,得到的差分电压值不是5V,只有3.3V的样子。当我全部给tdata输入为‘1’的时候,得到的数值跟上面的值一模一样。所以想问下问题出现在哪啊?时序没有错,我通过仿真检查了很多遍。