Part Number: ADS1219
Other Parts Discussed in Thread: TL074, TINA-TI, OPA657, LMP7721
我希望能进行微弱电流的检测(1-100nA),我对精度要求不高,误差±5nA都可以,我对采样速率和延时也没有太大的要求,因为我的信号是近似直流的缓慢变化电流,我看了ADS1219的采样是1000SPS,足够使用了,电路图在下面,我找不到ADS1219它的输入阻抗是多少,会不会有太大的分流。另外我现在很担心这样的设计会引入噪声使得原始电流信号被淹没,ADS1219会在输入端引入多少噪声。如果这个方案不可行的话,希望您能推荐一个放大器加ADC的组合设计,虽然会更复杂,但是或许会有更好的效果。补充一点,我希望待测位置的电压不要被抬得太高,所以电阻我选了10k欧姆,我的chip最大能容忍输出端电压在100nA的电流下抬高到10mV,非常感谢!