Other Parts Discussed in Thread: DAC8830
想做一个信号发生器,用FPGA产生正弦数字信号,然后选用DAC8830作为数字转模拟,但是我发现这样子搭起来的电路会有个随频率变化的杂波,电路图是根据DAC8830的pdf来画的,用fft看,发现FPGA端口给的数据也没有这个变化的频率,但是经过了DAC8830,就多了这个频率,虽然是比较小,但是这样子导致我做的正弦输出的波形有1%的抖动,上面的测试DAC没有外接其他的芯片,FPGA端跟DAC芯片也是隔离开了的
输出100KHz左右的正弦波的时候,有个30KHz的频率
输出90KHz左右的正弦波的时候,有个40KHz的频率
为什么想要的频率跟杂波的频率刚好想加为130KHz,这个是不是DAC芯片就是这样子渣的?