有谁知道TLC5510这个芯片模拟输入的是电压信号还是电流信号,若是电压信号其范围是0.6~2.6,是否必须将模拟电压升高到这个范围,典型应用中的那个49.9欧的电阻做什么用的 ,从运放出来的信号必须接个电阻吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
有谁知道TLC5510这个芯片模拟输入的是电压信号还是电流信号,若是电压信号其范围是0.6~2.6,是否必须将模拟电压升高到这个范围,典型应用中的那个49.9欧的电阻做什么用的 ,从运放出来的信号必须接个电阻吗?
数据手册的典型应用
要测400K,要将0~1.5V的模拟信号转换为数字信号,这个不接电阻电容直接接到模拟输入口。如果是REFB接REFBS,REFT接FEFTS,测量电压范围是不是只能是0.6V~2.V,0.6V以下的无法转换为数字信号,另外要要转换0V~2V左右之间的模拟信号,将REFB接地,REFT接REFTS可以不可以