Other Parts Discussed in Thread: ADS5407
在ADS5407这款芯片的外部输入某电压值之后,利用signal tap监测采样后的数据发现这些引脚测试的数据一直为高低变化的,但是却不是一直处于均匀变化的状态,请问AD输出的12路lvds信号可以通过signal tap进行观测吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: ADS5407
在ADS5407这款芯片的外部输入某电压值之后,利用signal tap监测采样后的数据发现这些引脚测试的数据一直为高低变化的,但是却不是一直处于均匀变化的状态,请问AD输出的12路lvds信号可以通过signal tap进行观测吗?
Airwill 说:楼主有没有弄错?
ADS5407是低功耗 12 位 500MSPS 双路模数转换器
手册也没有 signal tap
我知道手册上面没有说用signal tap,但是如果不用这个工具的话我应该通过什么方式来测量AD芯片的输出,以证明我的AD采集功能是正常的呢?谢谢啦
Seasat Liu 说:可以研究以下寄存器的0x3C,0x3D和0x3e
关于test pattern感觉datashee上面写的不是特别清楚,请问一下是不是说如果我把HP1设置为0,而0x3C,0x3D和0x3e分别设置为0x8000,0x0000和0x0000,那么AD输出的数据为全零,而0x3C,0x3D和0x3e分别设置为0xBFFC,0x3FFC和0x3FFC时,数据输出为全1。那么设置为0x9554,0x2AA8和0x1554的时候应该怎么理解呢,以及该芯片的自定义模式那块不知道该怎么去理解。谢谢