Other Parts Discussed in Thread: AFE5832LP,
I have encountered an issue while using the HSDC Pro software to control the TSW1400EVM evaluation module. When initiating control through HSDC Pro, the software attempts to automatically launch the GUI for the AFE5832LP, but an error occurs during this process. The GUI for AFE5832LP fails to launch properly when initiated from the HSDC Pro software, and I encounter the following error message:
Error 7 occurred at HSDC Pro Version Check.vi -> HMC-DAQ GUI Pro.lvlib:Main.vi in the Call Library Function Node
Possible reason(s):
LabVIEW: File not found. The file might have been moved or deleted. Verify that the file path is correct using the command prompt or file explorer.
It is important to note that when I launch the AFE5832LP GUI software directly, it opens without any issues, which indicates that the software is installed correctly and the files are present. However, this error only occurs when the AFE5832LP GUI is launched through the HSDC Pro software.
Could you please assist me in resolving this issue? It is critical for my application that the integration between HSDC Pro and AFE5832LP’s GUI operates flawlessly, as I rely on this setup for ultrasound echo signal acquisition and analysis.
Thank you for your assistance!