Part Number: ADC128D818
ADC128D818 will enter shutdown mode in LowPower mode. Can I use the one shot function at this time?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ADC128D818
ADC128D818 will enter shutdown mode in LowPower mode. Can I use the one shot function at this time?

您好。我们可以直接使用中文沟通。
是的,当器件处于shutdown模式或深度shutdown模式时,启动单次转换和比较周期,之后器件会返回其所处的相应模式。 使用这个模式的明显优势是较低的功耗,这是因为此器件运行shutdown模式或深度shutdown模式。通过配置寄存器09h bit0=1 启动单次转换。

可以,就是在shut down模式或deep shut down模式启用one shot 转换。
low power 模式下有Low Power Conversion Mode。参考下面的介绍:
The One-Shot register is used to initiate a single conversion and comparison cycle when the device is in shutdown mode or deep shutdown mode。
9.2.2.2.8给出了deep shut down模式下的配置顺序,可以发现ADC进入shut down或deep shut down模式后,第三步才触发one shot转化模式。