Part Number: DAC81402
从手册上可以看出Reset引脚拉高后1ms,即可开始配置寄存器并输出电压。
但实际情况却是Reset引脚拉高并等待12ms后,才能正确输出电压,请问这是什么原因?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,Power on reset之后,reset需要拉高1ms对其进行寄存器的配置,这是没问题的。
然后这里又描述了POR后,器件进入power down模式,所有通道和内部参考都处于power down模式,DAC的输出也是通过1Kohm到地。
所以这1ms没有包含并输出电压的时间。
想问下,reset 拉高1ms是否可以正常配置寄存器?

您好,上电->拉高Reset引脚->等待1ms-之后,先配置0x3寄存器,先将DAC power down 模式disable ,再去配置其他寄存器试试呢?
默认是power down 模式,我认为在上电POR后,先将其处于normal operation状态,再去配置其他寄存器。