Other Parts Discussed in Thread: TLC2543
TLC2543采集值不对,在基准位2.447V(电压表测出来的),7脚是信号输入,外部信号通过AD623数据放大再输入,在输入为零时,AD623的5脚电压作为输入信号;
在做实验时输入为零,AD623的5脚加一个0.5878—0.6172V,那么数码管上应该显示984—1033字显示,可是在调节AD623的5脚电压时,显示的AD数就是调不到1000字?这是为什么?
TLC2543驱动函数:
sbit _CS=P3^5;
sbit CLOCK=P3^6;
sbit EOC=P3^7;
sbit DA_IPUT=P2^4;
sbit DA_OUT=P2^3;
unsigned int AD_out()
{
unsigned char i;
unsigned int AD_value=0;
_CS=0;
CLOCK=0;
for(i=0;i<12;i++)
{ DA_OUT=1;
_nop_();_nop_();_nop_();
CLOCK=1;
_nop_();_nop_();
AD_value*=2;
if(DA_OUT) AD_value++;
CLOCK=0; }
_CS=1;
CLOCK=0;
wait(5);
if(AD_value>=2)AD_value-=2;
return(AD_value);
}
void INIT_2543(unsigned char com)
{ unsigned char n;
_CS=0;
CLOCK=0;
for(n=0;n<12;n++)
{ CLOCK=0;
if(n<8)
{
DA_IPUT=(bit)(com&0x80);
com=com<<1;
}
CLOCK=1;
}
_nop_();_nop_();
CLOCK=0;
_CS=1;
DA_IPUT=0;
}
unsigned int TLC2543(unsigned char com)
{ EOC=1;
_nop_();_nop_();
INIT_2543(com);
wait(5);
while(!EOC);
return AD_out();
}