Other Parts Discussed in Thread: TVP7002
- TVP7002 VGA 输入分辨率支持1280 x 1536吗?
- TVP7002 VGA 输入能自动侦察VGA信号所使用的分辨率吗?如可以则读哪些寄存器,有例子吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TVP7002
介绍资料称: 1600x1200 的精度
The TVP7002 is a complete solution for digitizing video and graphic signals in RGB or YPbPr color spaces. The device supports pixel rates up to 165 MHz. Therefore, it can be used for PC graphics digitizing up to the VESA standard of UXGA (1600 × 1200) resolution at a 60-Hz screen refresh rate, and in video environments for the digitizing of digital TV formats, including HDTV up to 1080p.