This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1254数据读取问题

Other Parts Discussed in Thread: ADS1254, ADCPRO

ADS1254数据读取有问题,自己百思不得其解,求支持,现将问题描述如下:

ADS1254芯片,采样率9600,参考电压2.5V,使用STM32 的SPI读取数据,用示波器看了,数据能够完整读出,将读取的数据直接在LabVIEW上显示,信号发生器输出直接接到ADS1254的输入端,幅度0.5V~1.5V,问题如下:

1、信号发生器输出100Hz正弦波,显示的波形中存在有规律的问题:

2、信号发生器输出1.3KHz正弦波,显示的波行像有一个较低频率的载波,按说应该是一个很密的波才对。

3、信号发生器输出2.8kHz正弦波,显示显示的波行像有一个较低频率的载波,