寄存器读写都正常,可是不知道为什么就是没有数据输出来,我只写了两个寄存器,一个是0X00,写入的是0X00.一个是0X03,写入的是0X6D。现在我采到的信号一直都是0X80,0X10,0X80,0X10.......我查了一下(行和场同步信号都有),这个是默认的信号,不对呀。我输入视频后还是这个信号。晶振我是按说明书上面接得,开始用得是无源晶振,不行后(我想可能是晶振的精度不够所以不行),我又换成了有源晶振还是不行。说明不是晶振的问题。然后我又认为是电源的问题,换了几个电源后还是一样(我的电源连接方法是所以地连接到一起的,只有那个1.8V模拟和1.8V数字电源正上面加了一个磁珠做隔离,以防干扰)。9号脚有时种输出的是27MHZ。
我现在不知道问题出在什么地方,芯片我已换过了,还是不行。我用得是TVP5150AM1,希望帮忙分析一下,谢谢了。