我现在有个项目需要将CVBS/av模拟信号转MIPI/LVDS数字信号,请问TI在这方面有什么推荐的芯片吗?谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我现在有个项目需要将CVBS/av模拟信号转MIPI/LVDS数字信号,请问TI在这方面有什么推荐的芯片吗?谢谢!
目前TI的CVBS输入的视频decoder或者AD芯片都处于NRND状态,并且没有可替换的,倒是有SDI转MIPI的芯片。
你好,以上你说的这些,有具体型号吗?我先看下具体的资料,谢谢!!还有如果我将AV转成SDI然后在转成MIPI/LVDS,这样的思路的话,两者间的桥接芯片,有哪些推荐的型号吗?谢谢!!
你好,有两个问题,具体如下:
1,NRND状态的芯片有具体型号吗?我可以先参考下,
2,如果按照AV转SDI,sdi转MIPI/LVDS这样的思路的话,之间的桥接芯片,有具体的型号吗?谢谢
以前的视频decode 像TVP515x系列的都能接受CVBS输入,现在基本上都处于NRND状态了,而DSI转LVDS的有SN65DSI83.dragon Lee 说:你好,以上你说的这些,有具体型号吗?我先看下具体的资料,谢谢!!还有如果我将AV转成SDI然后在转成MIPI/LVDS,这样的思路的话,两者间的桥接芯片,有哪些推荐的型号吗?谢谢!!
CVBS 转BT656, BT656 再转SDI/MIPI.
前者芯片一般用TVP5150AM1, TVP5147
你好,给你推荐一个比较符合你要求的高速率传输芯片 THCV231/236
THCV231可以将最高12Bit/pixel的LVCMOS并行信号转换为串行图像信号的发送端IC。最其具备大传输速率3.2Gbps的CML串行输出,可以将1080p60Hz的12bit摄像头图像信号通过一对双绞线或者一根同轴电缆进行传输。此外,可以通过双向的传输通道进行I2C信号传输。
THCV236/可以将THCV发送端IC输出的串行图像信号转换为最高32bit/pixel的LVCMOS并行图像信号的接受端IC。1080p60Hz的16bit的摄像头图像信号通过一对双绞线或者一根同轴电缆进行接收。此外,还具备一条可以用来传输I2C、UART或GPIO等串行信号的Sub-Link,向传输通道“Sub-Link" I2C/UART/GPIO(最高4条)
详细信息可看官网http://www.thine.co.jp/zh_cn/products/num_details/THCV231.html,我司可提供规格书、样片和技术支持,欢迎联系qq:2817821256 手机18682112448