Other Parts Discussed in Thread: SN74LVC4245A, SN74LVC8T245
使用三片LJ245A做5V--3.3V之间的电平转换,第一片和第二片的方向为3.3V-->5V,第三片的方向是5V-->3.3V,请问如下设计是否可靠:
(1)5V直流电源连接至每片LJ245A的VCCA,该5V直流电经AMS1117-3.3芯片输出3.3V连接至每片LJ245A的VCCB;
(2)每片LJ245A的/OE(输出使能)连接至ARM的某个GPIO上,由ARM的程序控制是否使能和何时使能;
(3)每片LJ245A的DIR(方向)连接至ARM的某个GPIO上,由ARM的程序控制电平转换方向是5-->3.3 or 3.3-->5。
第一片的B1~B8及A1~A8全部用完,第二片只使用了B1~B4及A1~A4,第三片只使用了A1~A2和B1~B2。由于手册有一句话“All unused inputs of the device must be held at the associated VCC or GND to ensure proper device operation.”,那么遵循CMOS器件未使用的输入管脚不浮空的原则,将第二片未使用的输入管脚B5~B8直接接地,第三片未使用的输入管脚A3~A8直接接地。
这样的一个方案是否可靠?可行否?请TI的大佬们确认,多谢!