This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1675,咨询1675工作在2M,4M时的一些问题

Other Parts Discussed in Thread: ADS1675

你好

因项目需要采用了贵公司的ADS1675芯片,发现只要工作在大于等于1M的采样率的时候,AD采集回来的波形就很烂,但是工作在1M以下的时候就没有问题,请问这个芯片在工作的时候一般需要注意一下什么吗,尤其是工作在1M以上的时候,除了差分模式以外还有别的地方要注意吗?

  • 这是一颗高性能 delta-sigma (  )  ADC. 可以工作到 4Msps

    • AC Performance:
      103dB of Dynamic Range at 4MSPS
      111dB of Dynamic Range at 125kSPS
      –107dB THD

    从这个数据看, 虽然高采样率的性能有所下降, 也差不太多.