Other Parts Discussed in Thread: ADS8684, ISO7641FC, ISO7641FM
我现在在调试ADS8684,但是ADC的输出引脚的波形在最后一个高电平会拖很长的尾巴, 这个不知道怎么回事? 我拍了照片,上面的是CLK波形, 下面的是OUT波形。 另外,ISO7641在输入信号10MHZ的时候,会把脉冲信号变成了锯齿波的样子, 但我看资料上7641可以传25MHZ的信号啊? 你帮忙看看! 谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
关于ISO7641, 想问下你使用的是ISO7641FC 还是ISO7641FM ? 供电电压多大,3.3V 还是5V?资料上ISO7641FC 的最大data
rate为25Mbps(Vcc>=3.3V ),也就是说12.5Mhz.