This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ads1220通道切换后采集会有一个不稳定的阶段。怎么破。

Other Parts Discussed in Thread: ADS1220

在使用ADS1220,使用环境为四通道,配置为两个差分。01差分和23差分。01通道采集1.024~2V信号。配置禁用PGA。23通道采集一个1-8mV的小信号。使用128倍PGA,其他配置一样,使用内部基准源,内部时钟,连续采集模式。两通道频繁切换(切换周期10ms),分别进行采集,采集时,当采集完23通道,切换到01(禁用PGA)通道,需要延时600us以上,才能采集正常。从01通道切换到23(开启PGA)通道,需要延时3ms左右,否则采集到的数据就会有几个不稳定的点(偏离正常值)。工作过程可以描述为:配置01通道采集参数—>发送开始采集指令—>通过中断判断采集完成—>发送进入休眠指令—>配置23通道参数—>发送开始采集指令—>通过中断判断采集完成—>发送休眠指令。如此循环15000次。造成上面问题有可能是什么情况。希望能够得到指导。