Other Parts Discussed in Thread: DDC112
正在使用TI的数据转换芯片ddc112U,需要将芯片控制在非连续模式下工作。附件是使用的时序图,时序图上方的数字的单位是芯片系统时钟CLK的周期,例如600则代表相应高、低电平持续的时间为600个系统时钟CLK的周期。目前系统时钟CLK=10MHz,则一个CLK周期为0.1us(对应某一侧的积分器积分时间是60us)。使用示波器检查PCB板上的CONV信号时序参数,与附件所描述的参数一致,同时也检查过CONV的切换时刻与CLK上升沿的同步大约在1ns的范围内,但是观察不到芯片给出数据有效信号(/DVALID),示波器测量/DVALID信号一直为高。
(1)请TI的工程师确认一下,用这个时序来驱动DDC112U以使其工作在非连续模式下,是否正确?
(2)如果时序正确,能够使DDC112U工作在非连续模式,那么芯片不输出数据有效信号(/DVALID)的原因可能有哪些?
(3)TEST管脚应如何处理?正常使用时,该芯片的TEST管脚直接接地呢、还是由MCU的一个I/O来控制?
谢谢!