Other Parts Discussed in Thread: ADS1240, ADS1241
Hi
We'd like to use the ADS1240 in our design and want to know it's power consumption in power down mode.
We do a test with following setup:
DVDD connected to 3.3V and AVDD / Vref is open.
The PDN pin is connected to ground to force the device in power down mode.
Crystal is not soldered, i.e., no clock input to the chip.
All other I/O and control pins are left open.
We measure the digital current, it is around 80uA and varies as we touch the device. It is quite different from the datasheet where it should be 0.5nA.
We don't know whether our test setup is correct or not, could you please provide us your test circuit for digital current and analog current measurement in power down mode?
Thanks!
Sibing