This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PSIEVM: 滤波输出性能变差

Part Number: PSIEVM
Other Parts Discussed in Thread: ADS8681, , OPA1612, OPA227

刚收到订购的PSIEVM和ADS8681EVM。验证ADS8681的动态参数时,发现PSIEVM信号通过滤波输出比BP输出(不经过2K滤波器,直接输出)更差。

PSIEVM设置的Vpp=11.88V,Offset=0V,Freq=2KHz,单端输出。

ADS8681EVM的跳线帽保持默认状态,未做调整。PSIEVM的JP4(SE_VCM)跳线连接GND,JP8(DIF_VCM)跳线连接GND。

PSIEVM的JP3、JP1跳线连接BP,此时ADS8681EVM测的动态参数THD≈-100,ENOB≈13.6

当我把PSIEVM的JP3、JP1跳线连接Flt,此时ADS8681EVM测的动态参数THD≈-62,ENOB≈10.1,很明显,连接至滤波输出后,谐波大了很多。

 

请问是否可以判断PSIEVM的滤波电路出了问题?如何修复?

  • 您好

    当2kHz带通滤波器被旁路时,使用不同的放大器OPA227直接驱动输出SMA连接器,该连接器可以承受高电容性负载。使用2kHz带通滤波器时,PSIEVM的单端输出由OPA1612驱动,OPA1612只能直接驱动几十pF的电容。

    观察ADS8681EVM,有一个330pF的电容器直接连接到输入端C1。我建议移除这个电容器,这样可以消除PSIEVM上OPA1612输出级的不稳定性。

  • 移除C1电容后可以了。Thanks Taylor。